Plug-in, Turn-on: Wearable Development will Gain an Edge in 2015
by Stephen Evanczuk for Mouser Electronics
Featured Products
Featured Suppliers
Related Resources
Targeting a mainstream market beyond fitness buffs and quantified-self hipsters, wearables will begin establishing themselves in
2015 as the
most important piece of personal electronics since the smartphone - even relegating that centerpiece of
individual tech to a secondary role. While not the first such device, the Apple Watch due to ship in 2015
provides a validating market presence that promises to significantly expand market awareness and competitive
offerings. For engineers charged with implementing new wearable products, 2015 will also bring growing pressure
to quickly solve the complexity of wearable design and deliver products able to achieve greater functional
capability at significantly lower power. Intended to serve this critical design need, wearable design platforms
will emerge as a key enabler of wearable product rapid development.
Wearable designs represent a unique challenge for systems designers with functional requirements as diverse as advanced
real-time
sensor-fusion processing, sophisticated application execution, and novel human-machine interface
features. At the same time, engineers must deliver these capabilities within a tiny footprint able to slip into
fashion-driven packaging - all the while worn comfortably from day to day with minimal need for removal for
battery charging, software updates, or other needs typical of an electronic product. Finally, engineers must
implement these sophisticated designs in record time to beat an increasingly frenzied rush to gain a competitive
foothold in a rapidly evolving market.
Figure 1: No longer the sole domain of quantified-self hipsters,
wearables will rush into the mainstream, requiring ready-made development platforms able to speed
time-to-market of new wearable products. (Source: iStockPhoto.com)
In this environment, wearable design platforms will emerge widely to speed time-to-market with pre-packaged
solutions to the most difficult aspects of wearable design. For instance, ultra-low-power design requires a combination of low-power ICs, hardware design
techniques, and software methods to achieve the lowest possible power consumption short of compromising
application functionality. Rather than spending time tuning designs for critical features such as low-power
operation, wireless charging, and others, engineers can take advantage of the design platform's built-in
solution, optimized for wearable applications.
Wearable design platforms package hardware and software in development kits intended to showcase systems
solutions backed by hardware manufacturers
and their partners. The centerpiece of these platforms is a tiny hardware module designed to serve as a drop-in
solution for all but the most specialized design requirements. While more such platforms will continue to appear
in 2015, two platforms likely to cause a stir in 2015 include the WaRPboard and Intel
Edison .
Expected to ship in early 2015, the WaRPboard reference platform represents the efforts of hardware, software,
and manufacturing companies to offer an open-source reference platform for wearable designers. Based on Freescale processors , WaRPboard hardware includes a main board fitted with a Freescale i.MX 6SoloLite ARM
Cortex-A9 core-based application processor and a daughter card using a Freescale Kinetis KL16 ARM
Cortex-M0+ core-based MCU for real-time processing. In this hybrid architecture, designers implement
their wearable application on the main board, using the daughter card for real-time tasks including sensor
processing and wireless charging . WaRPboard
addresses connectivity diversity required in wearables with built-in support for both WiFi and Bluetooth 4.0 .
The Intel Edison features a similar hybrid processor
architecture based on an Intel SoC that includes a dual-core 500 MHz Atom CPU for application processing and a
32-bit 100MHz Quark MCU for real-time execution. The postage-stamp-size board includes 1GB LPDDR3, 4 GB EMMC,
and 40 GPIOs configurable as a wide range of I/O peripherals including USB 2.0, UART, and I2C, among others.
Also supporting both dual-band WiFi and Bluetooth 4.0, the Intel Edison module includes a device-to-device and device-to-cloud connectivity
framework to enable cross-device communication and a cloud-based analytics service.
WaRPboard and Intel are by no means the only players in the wearable-reference design-platform game. For example,
Texas Instruments has offered its eZ430-Chronos
kit for years. Based on a 16-bit MCU with integrated sub-GHz RF, the eZ430-Chronos provides a complete
development platform including watch, hardware, and software. With its integrated-wireless capabilities, the
Chronos serves as a central hub for nearby wireless sensors, such as pedometers and heart-rate monitors.
Design platforms such as the TI eZ430-Chronos are unique in including a wrist- or arm-worn accessory, but
wearables can of course be housed in diverse packages and worn anywhere - not only in plain sight on the wrist,
but incorporated into articles of clothing, simply pinned to garments, or even stuck to the skin. Indeed,
engineers will find a growing number of wearable-reference platforms or simple-reference designs revolving
around ICs and IC chip-sets. For example, targeting for wearable medical applications , Maxim Integrated
bills its Wellness Platform as a suite of design hardware and software based on its WASP/MAX32600
MCU. In fact, engineers who would rather create their own design solutions will find a growing number of ultra-low-power MCUs designed specifically to meet
wearable-design requirements.
With enough time and expertise, an experienced design team can build exceptional wearable applications based on
these MCUs. Yet, time-to-market is a critical factor in the wearables market. For wearable-design companies and
design engineers, a key decision in 2015 will lie in balancing the possibility of product differentiation and
performance in building a wearable design based on these MCUs against the probability of quick market entry
using a wearable reference platform.
Stephen Evanczuk is a freelance writer with
more than 20 years of experience writing for and about the electronics industry. Currently working as a
freelance writer for electronics-industry companies and trade press, he writes about topics reaching broadly
across both industry issues and design challenges affecting engineers -- ranging from analog and digital design
to software and hardware for embedded systems. Prior to his freelance career, Evanczuk has worked in various
editorial positions at CMP (Editor-in-chief of High-performance Systems and section editor at EE Times), VNU
(Editor-in-chief of Engineering Tools), and McGraw-Hill (Microprocessor/systems editor at Electronics). Prior to
that, he worked at TRW (Redondo Beach, CA) as a performance analyst for a very-large scale distributed system;
as project manager for firmware optimization; and as a Staff Member for the TRW corporate R&D leadership team.
Prior to joining TRW, Evanczuk completed his doctoral work at the University of Pennsylvania, where he developed
a high-performance real-time distributed-processing data-acquisitions system and associated signal-processing
algorithms, which were later used in TRW ground-based signal-acquisition systems. Along with his freelance work,
Evanczuk is currently heavily involved in cloud-based distributed systems and apps development.